Ultrafast Laser Applications: Short Pulse Revolution
Join representatives from Edmund Optics, TOPTICA Photonics, and Rochester Institute of Technology for a virtual discussion about the key benefits of ultrafast lasers and how they are revolutionizing fields as diverse as brain imaging and glass polishing.
Choosing the Right Lasers and Optics for Ultrafast Microscopy
Join us for a discussion on selecting the best ultrafast laser sources and optical components for your ultrafast microscopy system to maximize performance.
6 Considerations for Medical Optical Device Development
Master the unique challenges associated with sourcing optical components to produce successful medical devices in this webinar with Edmund Optics experts.
Jeremy Govier, Principal Engineer, and Andrew Lynch, Expert Rapid Prototyping Solutionist, discuss 13 creative "hacks" to quickly and efficiently make prototypes of optical systems to address collapsing product lifecycles.
New optical filters are being developed due to the advancements in applications and technologies. Learn more about the future of filters at Edmund Optics.
Laser Induced Damage Threshold (LIDT) or Laser Damage Threshold (LDT) are crucial for selecting or specifying laser optics. Learn more at Edmund Optics!
Learn how Highly-Dispersive Mirrors compensate for dispersion and compress pulse duration in ultrafast laser systems, which is critical for maximizing performance.
Mounting flat mirrors by their edges in a kinematic mount imparts stress onto the mirror surface. This results in distortion and reduced quality of the reflected wavefront, which is especially noticeable when using high-quality mirrors. Stemmed mirrors, on the other hand, are mounted from a smaller diameter “stem” protruding from the back of the mirror, resulting in significantly reduced stress on the mirror surface, high stability, and cost reduction and can be used as a replacement for a more expensive and complex kinematic mount and a conventional mirror.
Athermal optical systems are not prone to temperature changes in an environment. Learn more about the importance of having an athermal design at Edmund Optics.
Single-Material Aspheric Achromats correct chromatic aberrations with a unique geometry, leading to numerous benefits over conventional achromatic lenses.
or view regional numbers
QUOTE TOOL
enter stock numbers to begin
Copyright 2023, Edmund Optics Inc., 14F., No.83, Sec. 4, Wenxin Road, Beitun District , Taichung City 406, Taiwan (R.O.C.)
California Consumer Privacy Act (CCPA): Do Not Sell My Information